Snell's Law | Terminology | Lens Geometries
Optical lenses are the most important tools in optical design for controlling light. When optical designers talk about optical lenses, they are either referring to a single lens element or an assembly of lens elements (Figure 1). Examples of single elements are plano-convex (PCX) lenses, double-convex (DCX) lenses, aspheric lenses, etc; examples of assemblies of elements are telecentric imaging lenses, infinity-corrected objectives, beam expanders, etc. Each combination is comprised of a series of lens elements and each element has a specific lens geometry which controls light in its own way.
Figure 1: Plano-Convex Lens (Single Element on Left) and Telecentric Imaging Lens (Combination of Elements on Right)
SNELL'S LAW OF REFRACTION
Before delving into each type of lens geometry, consider how optical lenses bend light using the property of refraction. Refraction is the means by which light is deviated by a certain amount when it enters or leaves a medium. This deviation is a function of the index of refraction of the medium and the angle the light makes with respect to the surface normal. This property is governed by Snell's Law of Refraction (Equation 1) where n1 is the index of the incident medium, θ1 is the angle of the incident ray, n2 is the index of the refracted medium, and θ2 is the angle of the refracted ray. Snell's Law describes the relationship between the angles of incidence and transmission when a ray travels between multiple media (Figure 2).
(1)
Figure 2: Snell's Law of Refraction [View Larger]
OPTICAL LENS TERMINOLOGY
All optical lenses obey Snell's Law of Refraction. Consequently, it is the optical lens geometry (i.e. the surface profile) that determines how light behaves as it propagates through the optical element. To understand the terminology used in optical lens specifications, consider 10 common terms (Table 1). For more detailed definitions and a list of additional terms, please view our Glossary.
| Table 1: Common Optical Lens Terminology | |
| Abbreviation | Terminology – Definition |
| D, Dia. | Diameter – The physical size of a lens. |
| R, R1, R2, etc. | Radius of Curvature – The directed distance from the vertex of a surface to the center of curvature. |
| EFL | Effective Focal Length – An optical measurement given as the distance from a principal plane of an optical lens to its imaging plane. |
| BFL | Back Focal Length – A mechanical measurement given as the distance between the last surface of an optical lens to its image plane. |
| P, P" | Principle Plane – A hypothetical plane where incident light rays can be considered to bend due to refraction. EFL is specified from a principal plane location. |
| CT, CT1, CT2, etc. | Center Thickness – The distance from a primary principal plane location to the end of an element. |
| ET | Edge Thickness – A calculated value which depends on radii, diameter, and center thickness of a lens. |
| db | Entrance Beam Diameter – Diameter of collimated light entering an axicon. |
| dr | Exit Beam Diameter – Diameter of ring of light exiting an axicon. |
| L | Length – The physical distance from end to end of a cylindrical element (e.g. cylinder lens) or the distance from apex to work piece of an axicon. |